Industry Online Support
Technical Forum
4/6/2006 10:51 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (150)
|
The current version of WinCC is 6.0 SP4[:o] I expect the only files needed from your existing machine will be your WinCC project directory. You will need to migrate your project from version 3 -> 4 -> 5 -> 6.There is no direct upgrade from V3 to V6. You will also need to upgrade your operating system to 2000, XP or 2003. Finally you will have to upgrade your hardware as WinCC V6 needs ~1.4Ghz and 500Mb RAM as a minimum. I would strongly advise you contact your local Siemens office. They will be able to advise you on the best method for upgrading with minimum cost and time. Here are some faqs to point you in the right direction: http://support.automation.siemens.com/WW/view/en/22020734 http://support.automation.siemens.com/WW/view/en/21927774 http://support.automation.siemens.com/WW/view/en/15342782 http://support.automation.siemens.com/WW/view/en/17356933 Regards, Salma |
4/6/2006 1:09 PM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (150)
|
If you do not know where your local Siemens office is then you can use the Contacts worldwidelink in the Contact box, located in the top right-hand corner of this site. |
Follow us on