4/30/2008 1:04 PM | |
Posts: 1776 Rating: (95)
|
Hi, try to start WinCC without User archives. Does it works? Maybe also try the FAQ http://support.automation.siemens.com/WW/view/en/26134057 |
4/30/2008 2:40 PM | |
Posts: 63 Rating: (0) |
Yes, its working fine n smooth and too when Alarm logging and tag logging are activated at the WinCC start up. I deleted the .dcf file from project path but still unable to activate the User Archives. Only getting problem with User Archive. I have attached the .pdf file, have a view. AttachmentUserArchiveProb.pdf (53 Downloads) |
5/1/2008 2:29 PM | |
Joined: 9/7/2007 Last visit: 8/30/2023 Posts: 550 Rating: (62) |
check the link below if you want to upgrade from WinCCv6.0 to WinCCv6.2 SP2 https://support.automation.siemens.com/WW/llisapi.dll?query=service+pack+2+for+wincc+v6.0&func=cslib.cssearch&content=skm%2Fmain.asp&lang=en&siteid=cseus&objaction=cssearch&searchinprim=&nodeid99= |
Best Regards |
|