4/11/2019 10:40 AM | |
Joined: 10/3/2010 Last visit: 4/29/2024 Posts: 1552 Rating: (188) |
Is there any way to use the "enable monitor keyboard" on a WinCC client in order to have only the NumPad visible instead of a full keyboard layout? It would be strange if not possible because users have been asking this feature for decades now. "CCOnScreenKeyboard.exe" I don't want to start this keyboard via command line nor by using a script! |
Last edited by: SteBo at: 4/11/2019 10:44:59 AMB r g d s , |
|
4/12/2019 5:18 PM | |
Joined: 6/26/2014 Last visit: 7/29/2022 Posts: 42 Rating: (2) |
These are the keypads supplied by USDATA to us after conversion from FactoryLink to WinCC. I never used them. AttachmentWinCC Keypad Document.zip (346 Downloads) |
4/12/2019 6:01 PM | |
Joined: 9/19/2009 Last visit: 4/27/2024 Posts: 458 Rating: (81) |
Hi Still you can use the old TouchInputPC.exe, see the sample, it is spanish but the code is the same Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
Follow us on