4/29/2009 1:01 PM | |
Joined: 4/17/2009 Last visit: 4/17/2024 Posts: 28 Rating: (0) |
Hi Phantom, Thx for your reply. I tried by saving and reorgnising the project but unfortunatly it didn't work. We are using this block for all other AI and alarm problem appearing on earlier mention two tags only.. Also i tried following method recomanded by support this also didn't work. - Please write down the message number of the not acknowledgeable messages - open the project on the ES - create a binary variable in the internal tags - please search for the message number in the alarm logging - in this message, please implement the message variable and safe - implement E/A fields in a process picture and connect this binary to the variable - download the server (delta) - on this server, please set the variable to "1" - the message should now get a new time stamp and should now be acknowledgeable
AttachmentWeired Alarms.zip (156 Downloads) |
5/7/2009 8:09 AM | |
Joined: 4/17/2009 Last visit: 4/17/2024 Posts: 28 Rating: (0) |
Hello experts, Anybody have the solution,suggestion or recommendation for mention problem in thread. Thanks, Regards, |
Follow us on