2/24/2009 1:06 PM | |
Posts: 510 Rating: (117) |
Here is the previous thread on your question. /tf/WW/en/Posts/24513 |
2/24/2009 4:34 PM | |
Joined: 1/16/2006 Last visit: 3/21/2024 Posts: 125 Rating: (50) |
Hi, if you have installed SP3 you only have to insert theregistry key from the attachment. So WinCC thinks you have installed KB319740. Now you can install WinCC. regards Cookie AttachmentKB319740.zip (3524 Downloads) |
This contribution was helpful to12 thankful Users |
3/18/2009 1:11 PM | |
Joined: 8/8/2008 Last visit: 12/14/2023 Posts: 78 Rating: (4) |
Many Thanks for posting the file. |
3/19/2009 3:32 PM | |
Posts: 1275 Rating: (123)
|
Hi Cookie, Has this fix been officially released by Siemens? Could you send me a link with the official release? On the compatibility list Windows XP SP3's still not included... There's a FAQ on how to uninstall SP3, though. Best regards, Danielle |
Last edited by: Danielle at: 3/20/2009 1:12 PM |
|
3/20/2009 1:23 PM | |
Posts: 1275 Rating: (123)
|
Hi Jaromir, I still hadn't read about v7.0 SP1! Thanks for the heads up on that one! So... here's the Delivery Release for WinCC v7.0 SP1 link and Siemens made the Service Pack available for download just yesterday! So here's the link for the download of SP1 for WinCC v7.0! Best regards, Danielle |
Follow us on