6/18/2008 5:15 PM | |
Posts: 2661 Rating: (279) |
Seems to me your problem is because the binding order got changed. You can adjust this as follows: Go to Network Connections from Control Panel. Then Advanced Settings and Adapters and Bindings tab. Also, you should try pinging using the computer name and not the IP address. TheIP address shown (after the ping) should be from the terminal bus network card and not the officeLAN network card. You may need to adjust the hosts and lmhosts file. The following FAQ's will prove useful too: How do you use the SIMATIC shell to configure the terminal bus of a WinCC station? How can you clear the error message "Download (310:88)"? Regards |
6/20/2008 1:55 PM | |
Joined: 12/8/2006 Last visit: 11/27/2023 Posts: 170 Rating: (26) |
hi vgd, i have replicated your wincc problem on my computer. Ifa wrong network adapter is selected in simatic shell wincc can not findthe startpicture at startup of the runtime. In this case wincc ask you to choose a startpicture. If the server package is loaded on the client you can choose a start picture of the server. But the runtime will not be loaded because thewincc client can not find the startpicture by using the wrong network adapter! (wrong network adapter in simatic shell). The using of simatic shell is not normally. Please atted the notes in faq http://support.automation.siemens.com/WW/view/en/25437381 |