Industry Online Support
Technical Forum
10/21/2008 8:23 AM | |
Joined: 9/7/2007 Last visit: 8/30/2023 Posts: 550 Rating: (61) |
Hi LAID1, Is the WinCC freshly installed, or it was working good and unfortunately something happened? |
Best Regards |
|
10/21/2008 11:21 AM | |
Joined: 9/27/2006 Last visit: 5/3/2024 Posts: 12257 Rating: (2666) |
Hello LAID1; Which version of Vista are you running? WinCC 7.0 requires Vista 32-bit Ultimate or Business. Do you have one of these versions? See point 3 (Supported Operating Systems) in the following document: http://support.automation.siemens.com/WW/view/en/29501428 Regards, Daniel Chartier |
10/21/2008 10:18 PM | |
Posts: 25 Rating: (0) |
hello DCHARTIER; my vista is HOME PREMIUM 32 bit, therefore, WINCC7 could'nt run on this system since they are not compatible. thank you for your help. |
Follow us on