1/9/2008 3:18 PM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
Hello How many S7-200 PLCs ( CPU-224 ) can communicate with WinCC Flexible 2007 running on a PC with CP-5611. The FAQ below give a limit of 8 CPUs for WinCC Flexible 2005. https://support.automation.siemens.com/WW/llisapi.dll/22309264?func=ll&objId=22309264&objAction=csView&lang=en&siteid=cseus&aktprim=0&extranet=standard&viewreg=WW&load=treecontent#A15405924 While WinCC Flexible Communication manual says only one CPU can be connected to one HMI. Further WinCCFlexible allows you to configure many more S7-200 connections and does not give any error in configuration. Cal anyone please clarify the situation ? Regards Navnag |
There is no such thing as the last bug in a program |
|
1/9/2008 4:51 PM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating: (121) |
Hi i can not realy comprehend what you say (sorry) ....Further WinCCFlexible allows you to configure many more S7-200 connections and does not give any error in configuration... => When i cinfigure more connections as allow, then i get a fault messages after generate the project (not during the configure!) ....While WinCC Flexible Communication manual says only one CPU can be connected to one HMI..... => I read, that the max. connection aredependent from the panel which you are use. I think the FAQ are OK (i hope) If not, then the best are you contact the siemens hotline. => http://support.automation.siemens.com/WW/view/en/15363798 regards, |
Follow us on