5/23/2009 6:57 PM | |
Posts: 2661 Rating: (279)
|
You should set some password (same for all machines). Windows does not like no password. Also, can you ping using computer name? Have you setup the hosts files properly? Please read thoroughly the following entry: |
5/23/2009 9:29 PM | |
Posts: 2661 Rating: (279)
|
See ifthe following FAQ's are helpful: |
5/24/2009 11:11 PM | |
Posts: 2661 Rating: (279)
|
When you change the computer name you should register this name in the SQL server. See the following thread: SQL Server WinCC v6.0I suggest you verify this for all computers (after closing WinCC/Simatic Manager etc.). Regards |
5/26/2009 6:58 AM | |
Posts: 32 Rating: (0) |
Thanks a lot for your reply, I read it but unfortunately I'm using SQL SERVER 2005 and I couldn't find the thing that explained in the PDF file.
Best Regards |
5/26/2009 9:42 AM | |
Posts: 32 Rating: (0) |
Dear Sir, When I open the download log file it says that something with following concept "It can not open wincc file because it is locked" Best Regards |
5/26/2009 9:51 PM | |
Posts: 2661 Rating: (279)
|
See if the following is helpful: How can you correct the error message "OS is currently being loaded from another ES"? |