2/21/2013 10:43 AM | |
Posts: 9 Rating: (0) |
hello, Excuse me english is not good How to process the image....how to word shift
|
2/21/2013 11:54 AM | |
Posts: 9 Rating: (0) |
ATT could not be located |
2/21/2013 1:41 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365) |
Is your selected CPU an S7 1200? |
2/21/2013 2:18 PM | |
Posts: 9 Rating: (0) |
yes s7-1200 1214c/dc/dc/dc |
2/21/2013 2:23 PM | |
Posts: 9 Rating: (0) |
s71200 word shift is not possible to |
2/21/2013 2:25 PM | |
Posts: 9 Rating: (0) |
Do you have sample application |
2/21/2013 4:55 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365) |
Hello again, As huggy_d1 mentioned, it is possible to implement such logic with SCL if you are familiar with.There should be: 1-binary signal to trigger data entry 2-Array to keep the original data(in/out) 3-Static array to keep the stored data in , by trigger move data one cell up in for loop and put new data in 4- while temporary data is ready transfer it to output again in loop I hope that helps Hamid Hosseini |
2/22/2013 9:08 AM | |
Posts: 9 Rating: (0) |
Do you have an example file tia portal |
2/23/2013 8:27 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365) |
Hello, I have not a sample for the mentioned application but suggest checking: 1-Overview of SCL program(for S71200) control statements 2-FOR statement 3-Array data type Or search all necessary material in the following manuals as I did: SIMATIC S7 S7-1200 Programmable controller SIMATIC S7-1200 Easy Book Good luck for developing the idea, and share any difficulty here. Best regards Hamid Hosseini |
Follow us on