1/7/2008 8:39 AM | |
Posts: 32 Rating: (1) |
Hi I have looked in the Hardware (see Att) Is it the resolution the thinking about. And what about Preset value if you want to preset a kalibrationvalue on a specific hight on the position sensor. Is'it bit 2 in the lower byte?. Do you have an step 7 code for an exemple (FC or FB or STL ....) Attachmenthardw.zip (606 Downloads) |
3/17/2014 8:07 PM | |
Joined: 6/20/2011 Last visit: 4/30/2024 Posts: 74 Rating: (7) |
Late reaction, But i was struggeling with this sensor last week i create an FB wich can be used if needed. AttachmentMTS_SERIES_R_DP.zip (730 Downloads) |
Follow us on