8/10/2019 7:21 AM | |
Joined: 5/6/2015 Last visit: 5/6/2024 Posts: 2 Rating: (0) |
Hello guys I use tag logging to archive several tags, such as “AI_001_PV, …, AI_009_PV ”. the acquisition cycle is 1 second for these tags in the ProcessValue Archive. I want to export some archive data to excel use provider, and the timestep in the query statement I set is 5 minutes, the command string is like this:
But time interval of the exported data is 1 second! This is not occur on all the tags, but only for several tags. And it’s not for all the time, but only for several certain time. For example, when I want to export tag “AI_002_PV”, how often the timestep I set, the result is always correct! when I want to export tag “AI_005_PV”, sometimes like the time between '2019-07-03 12:25:18' and '2019-07-03 13:20:59' ,how often the timestep I set, the result is also correct; but sometimes like the time between '2019-07-04 07:28:18' and '2019-07-04 08:25:59' ,time interval of the exported data is always 1 second! The time above is UTC time. ________________________________________ The software version as follows: WinCC: V7.4+SP1 ConnectivityPack: V7.4+SP1 ________________________________________ I have check the archive data in the database using onlinetable, time interval it stored is 1 second.(My timezone is +8:00, so the first column in the table is 15:28) (See attachment_01.jpg in attachment) I use another tool to show the archive data in the database, time interval it stored is also 1 second. (See attachment_02.jpg in attachment) And I try to export the logs to txt file, it is like this: (See attachment_03.jpg in attachment) The software version: (See attachment_04.jpg in attachment) Anybody help me, please! Attachmentattachment.pdf (76 Downloads) |
Last edited by: susan06260626 at: 08/10/2019 07:23:45Last edited by: susan06260626 at: 08/10/2019 15:44:36 |
|
8/17/2019 2:21 AM | |
Joined: 5/6/2015 Last visit: 5/6/2024 Posts: 2 Rating: (0) |
Thanks to bg2492 for the reply. I have installed the Update 11 and it's OK now. thank you! Regards |
Follow us on