1/4/2020 11:08 PM | |
Posts: 2 Rating: (0) |
I am using WZC-P250 converter for reading about 150 Calorimeter from Seimens , and I am facing a problem now where the converter yellow LED indicator is always ON (thats means that the slave devices are sending data even when the these devices connected on the M bus are emoved the yellow LED is always ON ,where it is written in the manual the yellow LED flash only when the slave devices are sending data through the M-Bus. So now the we have no readings. What is the problem with this WZC-P250 ? Or is normal to for the Readings LED indicator to be always ON ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/07/2020 09:40:41New subject after splitting |
|
Follow us on