2/24/2012 5:23 PM | |
Joined: 5/13/2008 Last visit: 12/18/2019 Posts: 836 Rating: (71) |
Hi Satish, maybe this application will satisfy you: http://support.automation.siemens.com/WW/view/en/49492528 |
Last edited by: The Body at: 2/24/2012 5:25 PMmfG / Best regards |
|
This contribution was helpful to1 thankful Users |
7/19/2017 12:28 PM | |
Joined: 10/5/2016 Last visit: 9/12/2022 Posts: 236 Rating: (7) |
How to do it in the WinCC 7.0 SP3 ? |
Last edited by: KCD at: 7/27/2017 3:40:07 PM |
|
8/20/2020 9:50 AM | |
Joined: 12/13/2018 Last visit: 8/20/2024 Posts: 6 Rating: (1) |
thanks to all Also for someone confused like i was, here is my explanation: Function Trend Control can plot x[],y[] arrays of points from an existing csv file stored on the machine
https://support.industry.siemens.com/cs/ru/ru/view/109481693/en uses a VB script, that takes those arrays, clears existing .csv, writes in a FOR loop to the .csv file (archive), does error messaging along the way then a screen with the Function Trend Control is updated to summarise 1) generate x,y arrays in PLC 2) establish connection to x,y arrays in HMI, historic data - .csv archive 3) copy the VB script 4) add an UPDATE plot button, that calls the VB script and updates the screen with trend 5) add trend and use the archive (historic data)
|
This contribution was helpful to1 thankful Users |
Follow us on