9/13/2010 11:31 AM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating: (56) |
Hi, If you've checked everything I've mentioned and they are in factory default mode I don't know what to suggest anymore except for getting somebody onsite with the apropriate knowledge. But are you really sure that the P1 LED is lit up greenif it's connect to either the switch or the the PC?If this is the case and you are able to discover other devices with the PST-Tool I would suggest to change the IP-Address of the PC to be sure that there is no conflict due to duplicated IP-Addresses. About the firmware updates there are 2 Hardware Versions for Scalance available from which each has it's own firmware. Either you have the old or you have the new. In both cases I'm almost sure that the devices are not update. Firmware downloads: Download for SCALANCE W-700 firmware update: Download of firmware update V4.3.37 Download of SCALANCE W-788 Firmware Update for "old HW": Download of Firmware Update V3.4.11 I also guess that there already was a configuration available in the devices due to the LED behavior you described. Or it is because of the devices are loaded with a firmware version lower then v3.0.x. |
Best regards, |
|
This contribution was helpful to1 thankful Users |