10/6/2016 2:54 PM | |
Joined: 11/14/2008 Last visit: 4/24/2024 Posts: 504 Rating: (22) |
Is activex object registered ? Please check next FAQ how to register... Which Panel are you using btw ? |
10/7/2016 8:44 AM | |
Joined: 11/14/2008 Last visit: 4/24/2024 Posts: 504 Rating: (22) |
Can you try using Excel Viewer OCX . May be this can help... or may be free excel viewer of microsoft could help |
10/7/2016 1:43 PM | |
Joined: 6/3/2015 Last visit: 2/19/2024 Posts: 37 Rating: (0) |
It is the excel viewer from microsoft , but how do you need to call it in the script (createobject) . Thanks in advance |
10/7/2016 2:59 PM | |
Joined: 11/14/2008 Last visit: 4/24/2024 Posts: 504 Rating: (22) |
With what you'll open this xlviewer/Excel Viewer Microsoft ? with a button or does it need to open after a certain action, certain time .. ? If it should be opened by clicking a button, you also could try to assign StartProgram Event to this button and try it that way. Or you could use 2.2 Script wizard - Function list as described in this FAQ : Which VBS information and programming aids are there in WinCC flexible? |
Last edited by: OmegaProjects at: 10/7/2016 3:05:15 PMUpdate with script wizard function list Last edited by: OmegaProjects at: 10/7/2016 3:06:09 PM |
|
10/9/2016 6:25 PM | |
Joined: 11/14/2008 Last visit: 4/24/2024 Posts: 504 Rating: (22) |
If you can save in csv format you could this example ? to get or set data out from/to your table... How on a Windows-based panel can you use a script to save and read out data in a text file? |
Last edited by: OmegaProjects at: 10/9/2016 6:26:17 PMLast edited by: OmegaProjects at: 10/9/2016 6:26:39 PM |
|
This contribution was helpful to1 thankful Users |
10/10/2016 12:36 PM | |
Joined: 6/3/2015 Last visit: 2/19/2024 Posts: 37 Rating: (0) |
I will give it a try soon , thx for the help ! |
Follow us on