6/29/2009 12:52 PM | |
Joined: 10/7/2005 Last visit: 9/20/2024 Posts: 3021 Rating: (1054) |
Hello Wincc just to be clear, is your HMI Panel connected downstream of (behind)the Y-Link? If so, I'm afraidit won't work as you can only connect DP Slaves behind a Y-Link (a HMIis a Class 2 Master). |
Cheers |
|
6/29/2009 12:57 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello,
Look at How do you connect an operator panel (WinCC flexible) to an H system (S7-400H) about MPI or PROFIBUS? Hope this will helps. Best regards Hristo Mihalev |
Last edited by: UMENCHO at: 6/29/2009 12:59 PMAgain I am too late... Cheers Fritz ;) |
|
6/29/2009 1:13 PM | |
Posts: 25 Rating: (0) |
Hi all, I think we cannot communicate MP(MULTI PANEL) with Y-LINK. We can communicate only with PP17 using Y-LINK. Please check this FAQ. http://support.automation.siemens.com/WW/view/en/22584323. Please check. bye karn |
7/2/2009 7:11 AM | |
Joined: 6/3/2009 Last visit: 6/24/2024 Posts: 101 Rating: (7) |
Dear Fritz I attached the configutation, this may help you. Attachmentconfi.zip (282 Downloads) |
7/2/2009 9:04 AM | |
Joined: 10/7/2005 Last visit: 9/20/2024 Posts: 3021 Rating: (1054) |
Hello Wincc I'm afraid my previous answer still holds true (you can NOT do this). Have a look at the links that Umencho and karn provided in this post as well as this and this thread which I trust willhelp. |
Cheers |
|
7/2/2009 9:39 AM | |
Joined: 6/3/2009 Last visit: 6/24/2024 Posts: 101 Rating: (7) |
Dear fritz Any other Possibility to communicate the HMI using the above configuration. |
7/2/2009 10:51 AM | |
Joined: 10/7/2005 Last visit: 9/20/2024 Posts: 3021 Rating: (1054) |
Hello again Wincc the short answer is: NO Asunderstanding is the key to appreciating why my answer is persistently negative, let me elaborate a little: The following statements arestraight from this manual: The Y link is slave on the higher level DP master system and acts as a proxy for the nodes connected on the underlying bus system (DP slaves). The Y link forms an independent underlying bus system that is decoupled from the higher level DP master system in terms of communication. In the underlying DP master system the two IM 153-2 (the Y-Link) use the addresses 1 and 2. The first possible address for an underlying DP slave is 3.
|
Cheers |
|
7/2/2009 11:03 AM | |
Joined: 6/3/2009 Last visit: 6/24/2024 Posts: 101 Rating: (7) |
DEAR fritz Please see the attachment and give me feedback that will work or not. AttachmentRE CONFI.zip (261 Downloads) |
7/2/2009 11:15 AM | |
Joined: 10/7/2005 Last visit: 9/20/2024 Posts: 3021 Rating: (1054) |
Dear WinCC I'm not to sure how to say this but you are going from bad to worse. Please stop guessing and start reading the information in the link that Umencho provided you with. |
Cheers |
|
Follow us on