5/17/2017 9:26 PM | |
Joined: 9/27/2006 Last visit: 4/23/2024 Posts: 12257 Rating: (2665)
|
Hello Zauberer; To answer your second question first, have a look at the following documents: What is the effect of the STEP 7 function 'Copy RAM to ROM'? Note: The third case discussed in the preceding document would apply to your CPU 317-2DP: SIMATIC S7-300 CPUs and SIMATIC C7 devices with micro memory card (MMC) How can you write the program to the FLASH Memory Card when using a SIMATIC S7-400 CPU? Now for the first part of your question. If you have non-Siemens equipment in your project, as part of a Profibus-DP network, they must have been integrated to the Profibus configuration using a file with a GSD extension (or .gse, or gs_); these files are not copied to the next computer when you transfer the program. You should copy them by hand. Normally these files are located in the Step 7 project tree, under data/gsd (but that will depend on the software version, so search for .gsd). Copy these files to the new computer, paste them in the same location and you should e=be able to run again. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 5/17/2017 9:27:54 PM |
|
This contribution was helpful to2 thankful Users |
Follow us on