11/26/2021 1:38 PM | |
Joined: 11/9/2021 Last visit: 3/11/2023 Posts: 3 Rating: (0) |
Hi All, I’m newbie in this filed. I have an issue with a project. Actually I’m trying to fix a machine in the glass industry. My problem is this: We have a DC motor with a bridge rectifier and voltage regulator. The motor is meant to rotate a table 3600 The start and stop of the table is on a limit switch for rotating left. Same goes for right rotation. The command of starting the table comes from a push button. I have tried different ways of doing it but it didn’t seem to work it out. Would anyone have the kindness of transposing the above on a program? Having this as a start I hope that I can finish up the whole project as it would still have the up/down commands etc. Thanking you for your kindness Laurentiu CretuAttachmentMotor rotation.zip (450 Downloads) |
Last edited by: CmTelectric at: 11/26/2021 15:30:11 |
|
11/27/2021 3:33 AM | |
Joined: 12/18/2014 Last visit: 4/23/2024 Posts: 32869 Rating: (4064)
|
Maybe this helps you a little bit ... |
Follow us on