3/6/2018 2:33 PM | |
Joined: 9/7/2017 Last visit: 9/18/2024 Posts: 5 Rating: (0) |
Hi, I have trying to configure the wincc/audit 7.4 SP1. I want to save the action from the operator, by push button. I have a problem a save the comment in Audit Database. First I used the script GcreateMyOperationMsg(). Using this script appear pop-up, but the message write in pop-up not saved into Audit db and any action is save as "Paste" and "Alarm (RT)". After I used the script InsertAuditEntryNew(), but in this case the message is saved, but is not possible to add any information about the action to do (open/close, Instrument TAG, ext). How is possible to save the description of the action and the comment from the operator? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/20/2018 8:58:07 AMNew subject after splitting |
|
Follow us on