11/16/2018 3:12 PM | |
Joined: 5/13/2012 Last visit: 1/17/2024 Posts: 179 Rating: (1) |
Dear Mike Many thank you understand me correctly . But when I ask the sales engineers from schnider ,the answe was our gateway convert the modbus RTU to Ethernet (without more details ),so right now I am confused from the answer. first scenario :I have attached an example of the gateway showing the main task by using address as an example ,waiting schnider conformation about it . second scenario :actually it is a question ,if the EGX 150 gateway works as protocol converter just as you said ,Modbus RTU to MODBUS TCP/IP ,it means the EGX 150 will convert the Modbus to TCP frames ,at this case I am going to use the SICAM PAS interfaces TCP/IP and the address of each energy meter on station address ,,so that I will add interfaces TCP /IP equal to the number of connected meter devices ???or what .see attached sicam PAS I hope now you can understand me correctly . the issue that I faced currently is that the schinder doesn't give me a details ,all information is schnider software can access and read all data from each meter through the EGX150 ,by insert the slave ID for each meter ?!! thanks and best regards Attachmentmeduim switchgear schnider explanation.zip (465 Downloads) |
Last edited by: fanana at: 11/18/2018 11:40:28 AMbest regards |
|
11/18/2018 11:42 AM | |
Joined: 5/13/2012 Last visit: 1/17/2024 Posts: 179 Rating: (1) |
attached the second SICAM PAS explanation photo. |
best regards |
|
1/20/2022 7:04 AM | |
Joined: 12/27/2018 Last visit: 3/20/2024 Posts: 7 Rating: (0) |
Hi Could you update the latest progress. I'm developing a same type of applications. |
Follow us on