7/31/2020 9:14 AM | |
Joined: 1/24/2015 Last visit: 9/12/2024 Posts: 1 Rating: (0) |
Hi, Siemens LOGO! 8 I want to compare two B007 & B016 counter only when the Output Q1 is high and not when it is low. I have converted the counter values to float using I/F block and then compare both with Analog compare. if both B007 & B016 counters are same and Q1 is high than i need to increment a counter B034. In the whole compare operation there is no En(enable) signal which i can control. How do i do this compare operation? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/31/2020 10:20:47New subject after splitting |
|