5/3/2012 12:42 PM | |
Posts: 557 Rating: (64) |
hello, The maximum size of the diagnostic buffer is a CPU property that can be set for certain CPU types. Displaying the diagnostic buffer in RUN mode can increase the scan cycle time. Some modules therefore display only some of the entries in the diagnostic buffer (default via module property). You can set a number for these modules that differs from the default number. Select "Default" and enter the value you require in the text box. Remember that the scan cycle time may be increased if you select a large value. Attachmentdia.pdf (1266 Downloads) |
This contribution was helpful to2 thankful Users |
5/6/2012 5:41 PM | |
Posts: 947 Rating: (45) |
need read message in diagnostic buffer, find adress error then see in hw-config area process image> which have same adress. Then find error |
Follow us on