7/17/2020 9:24 AM | |
Posts: 1 Rating: (0) |
hello, how can i compare the counter value? suppose i want to high the various output on the different-different counter value.. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/17/2020 09:46:20New subject after splitting |
|
7/17/2020 11:42 AM | |
Joined: 2/22/2008 Last visit: 2/22/2024 Posts: 2698 Rating: (206) |
If you want to compare 2 counters, then see example in attachment. You also can use it to compare with a fix value, then use e.g. counter1 without inputs to hold the fix value. Regards, Scorp Attachment2CounterCompare.zip (565 Downloads) |
Last edited by: Scorp at: 07/17/2020 11:42:39 |
|
7/17/2020 2:17 PM | |
Joined: 2/22/2008 Last visit: 2/22/2024 Posts: 2698 Rating: (206) |
Here is another option, a recursion with values>32767 is applicable with the converters I/F and F/I. I only have tried it in a simulation. Caution, don't use the VM area of the converters for other purposes. In the example the bytes VB0 up to VB7 are used from converters with type "double float" Maybe this recursion is also usable for other purposes. Regards, Scorp Attachment2CounterCompare V2.zip (271 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on