7/14/2020 3:48 AM | |
Joined: 1/2/2019 Last visit: 5/7/2024 Posts: 1 Rating: (0) |
How can I connect SIMATIC TI505 PLC with 505-CP2572 card? How can I set up IP and network parameter for the card ? What tools will be used to configure it ? Please give me some guideance Thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/14/2020 10:57:06New subject after splitting |
|
7/14/2020 4:27 AM | |
Joined: 9/27/2006 Last visit: 5/14/2024 Posts: 12257 Rating: (2668) |
Hello knightchi; You could start with the CP 2572 manual, it should give you much information on the installation, configuration and programming of the 505 Ethernet CP, using Tisoft (DOS-based) or some of its modern (Windows-based) successors, such as 505-Workshop. https://support.industry.siemens.com/cs/us/en/view/17519012 Section 2.4 of the CP 2572 manual give an example of the code required to connect a CP 2572 (Siemens 505) and a CP 343-1 (Siemens S7-300) over TCP/IP. Study this section attentively when you think you are ready to use the CP 2572 configuration and command word structure. If and when you need more information, feel free to visit us again to ask more detailed questions. Hope this helps, |
Last edited by: dchartier at: 07/14/2020 14:25:22 |
|
This contribution was helpful to1 thankful Users |
Follow us on