9/14/2020 12:57 PM | |
Joined: 12/18/2014 Last visit: 9/18/2024 Posts: 33790 Rating: (4197)
|
Please can you upload your programm as a Zip file? |
9/14/2020 6:18 PM | |
Joined: 3/30/2016 Last visit: 4/6/2024 Posts: 11 Rating: (0) |
Yes of course.AttachmentOpera di presa.zip (221 Downloads) |
9/14/2020 8:07 PM | |
Joined: 12/18/2014 Last visit: 9/18/2024 Posts: 33790 Rating: (4197)
|
I read the online help first. It says there that a program has a maximum of 40 I/O status names. And a maximum of 8 I/O status names in one message text. Then I created a small program and I was able to insert I/O status names in 5 message texts. Then I took your program and I was able to use 40 I/O status names there as well. Which firmware version has your LOGO!? Which LSC version use you? Attachmentsiriosystems.zip (232 Downloads) |
9/15/2020 6:04 AM | |
Joined: 12/18/2014 Last visit: 9/18/2024 Posts: 33790 Rating: (4197)
|
I have your program in a real LOGO! tested and now understand what you mean. Something is wrong with this file. Example: Message text SF012. In the program you can see that a status name is inserted in the 4th line of the message text, which should display the status of I11. In this simulation it is displayed, in the real LOGO! Not. Then I moved this status name to the 6th line, where it is also used in the real LOGO! not displayed. Then I inserted a new status name in the 4th line, which is then used in the real LOGO! also displayed. Then I deleted the old status name in the 6th line. The new status name is still used in the real LOGO! displayed. Very strange... Why?... I don't know... The changed program file is in the attachment, also screenshots in chronological order.
Attachmentsiriosystems_2.zip (226 Downloads) |
This contribution was helpful to1 thankful Users |
9/15/2020 8:49 AM | |
Joined: 3/30/2016 Last visit: 4/6/2024 Posts: 11 Rating: (0) |
I'm using LSC 8.2.0. I'm discharging LSC 8.2 SP1, maybe there was some bugs.... I will try. |
9/15/2020 12:59 PM | |
Joined: 3/30/2016 Last visit: 4/6/2024 Posts: 11 Rating: (0) |
The message not displayed is in SF013, input I15, Thank you. AttachmentOpera di presa.zip (234 Downloads) |
9/15/2020 2:13 PM | |
Joined: 12/18/2014 Last visit: 9/18/2024 Posts: 33790 Rating: (4197)
|
So, here too I made progress. At first I tried as with the message text SF012. You tried that without success, I noticed the same thing. Then I deleted SF013 and inserted a new message text, which again had the address SF013. Texts and status names inserted and in the LOGO! transfer. Result: Even worse, now the status names of I13 and I16 were missing, with I14 and I15 everything is okay. Then I first inserted a new message text (SF044) and only then deleted the old one (SF013). Texts and status names inserted and in the LOGO! transfer. Surprise: everything is fine now. Very, very strange everything.
AttachmentOpera di presa.zip (418 Downloads) |
Follow us on