4/11/2009 6:45 AM | |
Joined: 9/9/2007 Last visit: 8/12/2021 Posts: 27 Rating: (0) |
HI EVERY BODY |
4/11/2009 7:01 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, Look at Safety requirements Hope this will helps. Hristo Mihalev |
4/13/2009 9:23 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (306) |
Hello, The PFD can be found here: http://support.automation.siemens.com/WW/view/en/27832836 Here an example of: Practical Application of IEC 62061 Illustrated Using an Application Example with SIMATIC S7 Distributed Safety http://support.automation.siemens.com/WW/view/en/23996473 |
Best regards |
|
This contribution was helpful to1 thankful Users |
4/14/2009 8:36 AM | |
Joined: 3/24/2009 Last visit: 6/20/2023 Posts: 535 Rating: (112) |
Dear MDehshat, I think, that you want to calculate the SIL of your entire plant, don't you? In this case you have to find out all risk factors, which your system could bring, how often they appear and how you can avoid them. This will be the input for the SIL-calculation of your system. The PFD / PFH - values of the CPU / SM are only a part of the entire calculation. More information about Functional safety and the IEC61508 are available on http://www.iec.ch/zone/fsafety/fsafety_entry.htm Regards, yy1 |
4/21/2009 9:13 AM | |
Joined: 3/24/2009 Last visit: 6/20/2023 Posts: 535 Rating: (112) |
Dear MDehshat, I think the 'Safety Evaluation Tool' could help you: http://www.automation.siemens.com/cd/safety/html_76/produkte/si_normen/tool.htm Regards, yy1 |
This contribution was helpful to2 thankful Users |
Follow us on