6/18/2013 9:40 PM | |
Joined: 6/8/2013 Last visit: 1/29/2024 Posts: 188 Rating: (1) |
hi,,,,thank u of your help |
6/20/2013 12:43 PM | |
Posts: 1064 Rating: (72) |
It should have no effect at all except to free up memory (fill in memory holes from edits) |
This contribution was helpful to1 thankful Users |
6/24/2013 6:44 PM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating: (71) |
Hi Just to elaborate on whatcjustice said below is the excerpt from Step 7: The size of the work memory which can be used for logic blocks and data blocks can be altered by changing any of the following parameters:
You can have a look at attached file for more fun. AttachmentWork Memory.pdf (496 Downloads) |
This contribution was helpful to1 thankful Users |
6/25/2013 7:42 AM | |
Joined: 9/2/2012 Last visit: 3/22/2024 Posts: 711 Rating: (30) |
Dearcjustice, can you please eleborate You process image area for the input and outputonly really needs to be as large as your max I/O address can you explain with some examples mentioning address range and corresponding process image size ?? regards Vipz
|
|
|
Follow us on