7/3/2013 12:46 PM | |
Posts: 39 Rating: (9) |
Hi, What is the actual purpose of using Y_LINK In PLC? |
7/3/2013 12:54 PM | |
Joined: 9/27/2006 Last visit: 4/26/2024 Posts: 12257 Rating: (2665)
|
Hello chet; There is a very good explanation of the use opf a Y-Link as a gateway between redundant H-system CPUs andstandard Profibus slaves in the following FAQ: Description The Y link creates a gateway from a redundant DP master system to a unilateral DP master system. More information can be found in this manual on Profibus network interfaces: SIMATIC Bus links DP/PA coupler, active field distributors, DP/PA Link and Y Link |
This contribution was helpful to4 thankful Users |
7/3/2013 1:12 PM | |
Joined: 9/16/2011 Last visit: 9/10/2022 Posts: 291 Rating: (6) |
Good explaination bydchartier A little bit more to be added....... why Y-link called Y-link ?
see attached. |
Reg, |
|
This contribution was helpful to1 thankful Users |
Follow us on