9/6/2019 4:29 AM | |
Joined: 9/9/2015 Last visit: 9/15/2024 Posts: 727 Rating: (278) |
There are two types of "Ready" , one is IS ready, another one is PH Ready. It stands for Information Server and Process Historian. If you have Process Historian, you will need PH-Ready installed in the OS to pass the tag logging and Alarm logging data to process historian. If you have Information Server (for report generation) but not process historian, you will need IS ready installed in OS to pass the tag logging and alarm logging to Information server for report generation. Hope it helps. To read more information on Information server , click here . To have all the manual for PCS 7 , click here. Hope it helps. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to2 thankful Users |
Follow us on