11/28/2021 4:55 PM | |
Joined: 9/27/2006 Last visit: 4/19/2024 Posts: 12256 Rating: (2664)
|
Hello Ashu; The S7-1500R/H can only be servers on the S7 Communicaton, as you can see in the following screenshot, taken from the s7-1500R/H redundant system System manual. https://support.industry.siemens.com/cs/ww/en/view/109754833/141403261579 If you intend to use PUT and GET (S7 Communication functions) between your redundant S7-400H system and the S7-1500R/H, the S7-410H CPUs must therefore act as client, as explained by our friend Towone recently, in this discussion: Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
11/29/2021 7:48 AM | |
Joined: 9/5/2017 Last visit: 3/10/2024 Posts: 21 Rating: (0) |
hello Daniel, thanks for the response and got helpful information. we are in initial stage of architecture designing, planned to communicate multiple vendor package(s7-1515R-2N ) data to main package plc s7 410-5h,unfortunately s7 communication blocks are disabled for this plc in TIA v16. Open user communication blocks only enabled, if i get any manual or else sample backup means highly helpful to proceed Thanks and Regards, Aswanth Krishnasamy |
Follow us on