12/29/2021 6:49 AM | |
Joined: 4/10/2021 Last visit: 3/21/2024 Posts: 70 Rating: (6) |
Hi Anyone can please help about the problem in above post ???? |
1/11/2022 7:51 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating: (217) |
Hi ALI_N23, when the time at the alarm is not correct at the alarm is not correct please check the time at the CPU. The time at the CPU has to be in UTC and without any time zone. For more information see the manual PCS 7 Time Synchronization (V9.1). And whenever the batch string is empty it will displayed with "??". And the X with the blue background is a sign for at you can use the function loop in alarm, With regards |
This contribution was helpful to1 thankful Users |
Follow us on