1/11/2022 1:26 PM | |
Joined: 6/24/2018 Last visit: 7/8/2023 Posts: 3 Rating: (0) |
There is a bug in the insertion signal Is there the same problem PCS7 V9.0 SP3 |
1/12/2022 3:22 AM | |
Joined: 6/24/2018 Last visit: 7/8/2023 Posts: 3 Rating: (0) |
This is correct |
1/12/2022 8:09 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi, Have you defined the technological I/O as "Signal" type? see attachment. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
1/12/2022 9:35 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
You can find this setting in the technological editor when configuring CMT/EPHT/EMT. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on