1/27/2022 7:55 PM | |
Joined: 2/23/2021 Last visit: 1/9/2023 Posts: 1 Rating: (0) |
Hi, read the comments, my question is how many TCP connections can the S7-1200 make? I need 45 IPs in Modbus TCP/IP, thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/28/2022 10:29:31Edited text for better reading. Last edited by: Jen_Moderator at: 01/28/2022 10:30:21New subject after splitting |
|
1/28/2022 10:34 AM | |
Joined: 7/9/2015 Last visit: 8/30/2024 Posts: 3943 Rating: (585)
|
Hi, S7-1200 can 8 to maximum 12 connections (OUC). Check this: With which devices can the S7-1200 communicate via the integrated PROFINET interface and which protocols does the S7-1200 support?
Regards, Towome |
Last edited by: Towome at: 01/28/2022 10:35:41
|
|
1/28/2022 11:14 AM | |
Joined: 3/30/2020 Last visit: 9/19/2024 Posts: 4771 Rating: (981) |
Hello. The solution to your problem is to use 'dynamic' connections. Defining a TCP connection in the hardware configuration makes the connection a fixed connection. When the communication instructions define the connection (IP address and so on), then the connection becomes dynamic. A dynamic connection has the ability to be redefined.. There is a limit of how many connections can be open at any one time (as mentioned by Mr. Towome). But you can cycle through all the 40 devices within a time-span. Study what you can use from the helpful communication library: ~ |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to2 thankful Users |
Follow us on