10/18/2017 2:03 PM | |
Joined: 8/14/2013 Last visit: 4/11/2024 Posts: 47 Rating: (0) |
Hello, I use PUT/GET just like in example: The only change is timer M60 instead of M10. And I transfer data from db200 to db200 instead of mixing the numbers (I've tried mixing like in an example, the result was the same) The communication is between 317-6FF04-0AB0 and 410-5AX08-0AB0. And PCS7 is used on both sides. When I tried to transfer data like in example - Array of 20 bytes, it was successful, but when I try to transfer struct of bytes and reals (shown in example) I have no success. I always get 0 on both sides. Connection is present and in status it shows GET_NDR = 1. Any ideas what is missing? As I see in example, there is instance DB100 of FB100 in both PLC. Why is that? I tried to transfer array of REAL instead of bytes and communication went into error immediately. Any thoughts are welcome. Thanks AttachmentPUT_GET.zip (140 Downloads) |
Follow us on