10/19/2017 10:18 AM | |
Posts: 34 Rating: (0) |
Do you think I can use another network teaming software instead of SOFTNET-IE RNA ? |
10/19/2017 10:46 AM | |
Joined: 8/3/2009 Last visit: 9/20/2024 Posts: 13753 Rating: (1735) |
Hello Amen Allah in PCS7 this solutions are released and documented. Please look here: https://support.industry.siemens.com/cs/ww/en/view/61189687 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
10/20/2017 8:24 AM | |
Joined: 6/14/2006 Last visit: 6/17/2024 Posts: 301 Rating: (60) |
Hi Amen Allah, Intel Team mode is only used for the fault tolerant redundant terminal bus. In Netpro you do not configure anything about terminal bus. Terminal bus is configured by means of Windows network and the Intel teaming software. So nothing to do in Netpro for the terminal bus. ATTENTION: If you speaking about using PCS 7 V9.0 Intel teaming mode is not longer supported. Only RNA can be used! Please find the most actual version of the manual Murof linked: https://support.industry.siemens.com/cs/ww/de/view/109746538/en?dl=en Regrads |
This contribution was helpful to1 thankful Users |
10/20/2017 4:55 PM | |
Posts: 34 Rating: (0) |
Even not the affectation of the IP addresses ? |
Follow us on