6/20/2018 6:03 AM | |
Joined: 12/18/2014 Last visit: 3/28/2024 Posts: 32630 Rating: (4044) |
One last try ..... Otherwise, I have to see if one of my colleagues has TIA V15. AttachmentSample LOGO! as client and S7 as server.zip (118 Downloads) |
6/20/2018 6:06 AM | |
Joined: 12/18/2014 Last visit: 3/28/2024 Posts: 32630 Rating: (4044) |
One question? Do you use the same connection for HMI and LOGO! or have you different connections? |
6/20/2018 7:35 AM | |
Posts: 1283 Rating: (105) |
Two different connection defined. I had made a screenshot with highlight of both connections. Because my second PLC is not S7 series you cannot see a PLC image. that is the difference. So two connections,one HMI connection and one LOGO connection. Hope it is clear. Jay AttachmentConnections.doc (136 Downloads) |
Follow us on