4/27/2020 1:57 PM | |
Joined: 4/28/2015 Last visit: 7/9/2024 Posts: 3 Rating: (0) |
I have a Gen 4E 4000HP drive used for soft Starting a 3300kW screw Compressor . The Up-transfer permit was successful during the No Load Trial run. During the Load Test, the up-transfer permit does not work even after applying the Up-transfer Pulse was 60 seconds . The phase lock is not happening . Suggest a solution ! Please refer to the Screen shot and Event Logs and my sync Transfer Setting AttachmentForum Support for Up-Transfer Failure.pdf (438 Downloads) |
Amir Sharif |
|
4/28/2020 8:42 AM | |
Joined: 4/28/2015 Last visit: 7/9/2024 Posts: 3 Rating: (0) |
Dear Will, Thanks a lot for your input, i will give it a try and check. |
Amir Sharif |
|
Follow us on