12/11/2011 7:34 PM | |
Posts: 1 Rating: (0) |
Hello, I am working on CPU 314C-2 DP ( 6ES7 314-6CH04-0AB0/v1.0) with CP 343-1 Advanced (6GK7 343-1GX30-OXE0/V1.0). In my project, there are 2 CPU 314 with same hardware configuration with CP 343-1 Advanced. I am trying to establish a Connection between these 2 CPU using Netpro on a simulation with PLCSIM. At first I was using FC5 and FC6 to control the comunication but it didn´t work, then I read that PLCSIM (v5.4.4) doesn´t work with FC5 and FC6. Now I know I must use FB8/9 or FB12/13 or FB14/15 but I can´t make it work. For Example, I need to send AW124 in one PLC to EW124 in the other PLC and vice versa, can help me someone sending to me one sample program like these to run under PLCSIM (using CP 343-1 Advanced)? Please I need it , I tried it for two weeks, i don´t know how to do it. if you can help me i´ll be gratefull forever (and by the way , i´ll be able to sleep). Thank you very much and sorry for my english. I tried with this https://support.industry.siemens.com/cs/ww/es/view/18516182/en but i dont understand how to send and receive AW124 and EW124. |
Last edited by: Jen_Moderator at: 11/27/2017 1:20:19 PMInserted right link. |
|
12/12/2011 8:58 AM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181)
|
Hello, Try it http://support.automation.siemens.com/WW/view/en/38726591 The idea is "adjust" the hardware in order to simulate the software. Best regards, Hristo Mihalev |
4/25/2014 1:16 PM | |
Posts: 9 Rating: (0) |
hello my friend,s7 simulation don't support CP 343,you can only simulation Ethernet Communication via PN intergrate in CPU |
11/27/2017 1:21 PM | |
Joined: 6/19/2017 Last visit: 4/23/2024 Posts: 7956 Rating: (162) |
New question published by Jsalazar is split to a separate thread with the subject Simulate profinet communication. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on