4/7/2019 12:43 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Please refer What is a hardware interrupt and how do they work in the S7-300 system? FAQ which may help you. |
Last edited by: Jen_Moderator at: 4/8/2019 11:47:51 AMOptimized link. |
|
4/7/2019 1:02 PM | |
Joined: 4/17/2018 Last visit: 2/26/2024 Posts: 262 Rating: (60) |
Thank you for your reply, I read this link before and I read many topics talking about hardware interrupt, but I don't understand how it works regarding my previous attachment? |
4/7/2019 6:19 PM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
Here's an extract: "Program each channel group separately. The parameters can be changed at any time (in Attachment7BH01.pdf (333 Downloads) |
Last edited by: Kal.A at: 4/7/2019 6:39:30 PM |
|
4/7/2019 8:13 PM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
Here's one more attachment. The parameters of the module can be changed in runtime, i.e. in your user program. That is done by writing the relevant record with the modified parameters to the module. So if you look closely in your program you should find SFC57 (if not may be SFC55) and you should also find code that changes the channel parameters. The information is scattered across several manuals and you will need to dig-in further. AttachmentExtracts.zip (301 Downloads) |
This contribution was helpful to1 thankful Users |
4/7/2019 8:52 PM | |
Joined: 4/17/2018 Last visit: 2/26/2024 Posts: 262 Rating: (60) |
I'm looking in the program and there is neither sfc55 nor sfc57 |
This contribution was helpful to1 thankful Users |
4/7/2019 10:20 PM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
It's got me interested enough that I intend to look deeper into it later. If you need a quicker answer I would read more in the manual as it looks like the only way to address the module is to write records to it using some SFC of which their seem to be a few that may do the job. Attachmentextract.pdf (295 Downloads) |
Last edited by: Kal.A at: 4/8/2019 1:13:35 AM |
|
This contribution was helpful to1 thankful Users |
Follow us on