10/31/2018 7:03 PM | |
Posts: 12 Rating: (1) |
Hello! I have to establish a connection between Siemens S7-300 PLC and IOT2020 . For this project i bought an isolated module ETH-MPI but I can't connect the PLC and the Gateway . I bought this module because is cheaper than a Communication (PROFINET) Processor . I want to ask you if i can connect the PLC with the Gateway directly ( via USB) or there is a n another cheap way to assign an IP address for the PLC to make the connection normally Thank you very much ! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/5/2018 6:40:24 AMNew subject after splitting |
|
11/5/2018 6:41 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject Siemens S7-300 PLC - IOT2020 (ETH MPI-Isolated Module) is published within the conference IOT2000: Hardware & Interfaces.
Jen_Moderator |
Follow us on