11/19/2021 7:26 PM | |
Joined: 5/16/2016 Last visit: 4/19/2024 Posts: 41 Rating: (7) |
Problem Description When I execute a compile with "Generate module drivers" the driver interconnections are deleted for all FbDrive blocks in the project along with the generated charts and blocks (charts that start with @ symbol and contain MOD_DRV blocks). My first troubleshooting steps were to delete the IO interconnections (PZDIn1, PZDIn2, PZDOut1, PZDOut2) and complete a compile and download. I then reconnected the IO interconnection for PZDIn1 per the "Configuring frequency converters with FbDrive APL channel block SIMATC PCS7 v9.0" document. Per the document, the remaining connections (PZDIn2, PZDOut, Mode, DataXchg, etc) will generate automatically. However when I make the PZDIn1 connection the CFC editor closes, when I try reopen the chart I get notice the chart is open already. My guess is that the CFC editor is try to generate the the module drivers but is getting hung up. I read through FbDrive document to ensure that I have the correct HW setup and settings, I did not see any discrepancies. I also opened block driver settings and referenced PCS7 APL v90 library, but nothing changed. To work around this I restored an archive that contained the project with the module drivers. I downloaded that to the CPU without module generation. Detailed Info Urgency: fairly urgent, not able to generate module drivers PCS7 Version: v9.0 SP 2 - see attachment for details Operating System: Windows Server 2021 Build 14393 Is application Migrated? : The project in question was imported into existing MP Not sure what version. How often does the problem happen (Always/Often/Once/Not applicable)? Every time I run a compile the modules drivers are deleted. Every time I try to add the interconnection, the CFC editor crashes Is there a workaround. had to restore old project with drivers and download to PLC Did the function/functionality previously work? If yes, did something change recently (Windows update, PCS7 update etc.)? Archived projects have the module drivers, they delete when I compile with module generation. I joined the company after the project was made so I am not sure if worked previously. But I have been told that integrator created the project on separate stations and imported them into the current MP(Multi-Project) MLFB number (in case it applies to hardware) Danfoss FC302 VFDs (130B1135) Firmware version (in case it applies to hardware) GSD version GSDML-V2.32-Danfoss-FC-20171201.xml AttachmentInstalledESSW.pdf (358 Downloads) |
Last edited by: SilicornValley at: 11/19/2021 19:27:22Why you troubleshoot? |
|
11/24/2021 2:17 PM | |
Joined: 1/11/2019 Last visit: 4/23/2024 Posts: 684 Rating: (139) |
Hi, I have gone through the Installed software list which you have attached. Your libraries are older compare to the released updates in the market. Module generate driver blocks are generating from Basis Library block. You could try by installing the Update collection of released updates. Kindly go through the below link SIMATIC PCS 7 V9.0 SP2 Software Updates Note: Installation guidelines
Hope it helps you! |
This contribution was helpful to1 thankful Users |
11/27/2021 8:35 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Hi, I believe certain libraries or software packages were not installed in your engineering station. You have to look for the installed softwares and installed features in the previous engineering stations and do the comparison. Install all the relevant libraries, GSD, softwares that are related. You can also identify all the VFD, softstarter, DOL you have in your projects, ensure all the relevants GSD and Libraries are installed in your new stations. After identify, you must document them in you FDS or Maintenance manual to let everyone know that all those libraries and GSD must be made available in your project. Hope this helps you. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on