5/26/2011 8:17 AM | |
Posts: 8946 Rating: (999) |
[beware ironic] Dear friends, I also like to say, that I just do herea point-collecting post without further new information. It is just for increase my points, there is no need for reading or answer. But it would be a good idea to give em thanks and stars in order to increase my points much more, right!? With that in mind I like to say that I hope you all enjoy the campaign an keep on doing the good work! Here is also a link: /tf/WW/en/Posts/57932#top [/beware ironic] Sorry but I could not resist. |
This contribution was helpful to1 thankful Users |
5/26/2011 1:27 PM | |
Posts: 2661 Rating: (279) |
Sorry IBN-Service, couldn't resist thanking you and giving you the "stars"! Regards |
This contribution was helpful to1 thankful Users |
5/27/2011 8:35 AM | |
Joined: 10/7/2005 Last visit: 4/20/2024 Posts: 3004 Rating: (1046) |
Dear all to begin with, even though the amount of unnecessary "chatter" does increase in every Premium Campaign, the Campaign does achieve what it sets out to do. As for improvements,I like to take up an idea/proposal that IBN-Serviceessentially started some years ago when he suggested to make it possible to donate the premiums to a charitable organisation. The reasons (excuses?) for not implementing this were given as of practical/logistics manner. To overcome this and to allow Siemens to be a good corporate Citizen, here isidea on what to implement for next years Premium Campaign: 1.) Instead of a "lottery" Camcorder price for every 250 Premium points that one achieves,250 EURO's are accruedin the users name. At the end of the Campaign, Siemens will donate the money that each user accrued to a non for profit charity of the userschoice (alternatively, Siemens sets up a list of supportable charities that the users can pick from to avoidarguments about the "charitable character" of the chosen charity). 2.) Ideally as an addition to theabove (alternatively instead of theabove), the first10 placed at the end of the Campaign get 10000, 9000, 8000 --> 1000 EURO to donate. What do you say Siemens? We all help and support each other here which is great and this is the place to be as faras Siemens Automation related technical issues are concerned (alsolargely due to the work you Moderators do here, which often goes unnoticed). This is however THEopportunityfor Siemens to extend the reach of the Forum and to help those in real need (while we continue to help those who have the luxury toworry about how to format an MCC, connect a Drive to an S7, convert an S5 etc. etc.). Additionally, a nicely formatted "Siemens Technical Support Forum's Premium Campaign" Newsletter with pictures in it about the handover of the cheque's to thecharity organisation would show off Siemens as a good corporate citizen and should attract more users to this Forum. All up, its a ""win/win/win" situation for Siemens, the users here and those less fortunate than us. P.S: Excuses like "we don't have a couple of 10000 EURO's left in our budget"are not acceptable as an answer (and I can not think of any other reasons tonot implement this). |
Cheers |
|
This contribution was helpful to3 thankful Users |
5/27/2011 9:29 AM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
Uuaaaooo (sorry for my way of starting), |
5/27/2011 11:09 AM | |
Joined: 10/7/2005 Last visit: 4/20/2024 Posts: 3004 Rating: (1046) |
I find it VERY counterproductive to say the least and NOT in the interest of those whoI had in mind of helping. People will simply post their questions in another forum or not ask question at all,as it will also create an administrative overheadI am hopeful thatSiemens willignore thisidea. No problems though with Siemens making a "donation" button available during thecampaign where users can donate additionally to the overall sum made available by Siemens. |
Cheers |
|
This contribution was helpful to1 thankful Users |
5/27/2011 12:53 PM | |
Joined: 8/25/2006 Last visit: 4/19/2024 Posts: 2203 Rating: (277) |
I didn't understand you, what you mean? |
Follow us on