11/16/2021 4:11 PM | |
Joined: 1/11/2012 Last visit: 11/16/2022 Posts: 45 Rating: (3) |
Hi Jaz, I've face same issue with PCS7 V9.0 SP1 with Library, My project is migrating from PCS7 V8.0 to V9.0, the different is while you are using F system block, we use Power Control Library block, but I think the main issue is same, during compile process the result is error with "something cannot defined" description. Never tried your solution, but we will, so do you mean about absolute address, we don't need to assigned symbol, in symbol table, for example: IW2021, we just directly connect to our channel driver block chart, right? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/17/2021 10:29:48New subject after splitting |
|
11/17/2021 2:48 PM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Hi iamgroot , do you mind share your installed software and the error screenshots? seem like yours is different issue. did you install the power control library from siemens? you should have a installation exe for it. After you installed, your installed software should have this library and your register list (regedit) will have all the relevant module driver information which help you to compile necessary module driver. Hope this is helpful for you. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
11/18/2021 12:23 PM | |
Joined: 1/11/2019 Last visit: 4/23/2024 Posts: 684 Rating: (139) |
Hi, Power control V9.0 is compatible with PCS7 V9.0 and higher Please find the below link V9.0 SP1 Release note SIMATIC PCS 7 PowerControl Version 9.0 SP1 Update 1 After installing power control V9.0 pls do and check the following 1. Updated all the Advanced, Basis, Sirius and Power Control library blocks. 2. Connect to a correct symbol connection with absolute address link to hardware module And, check in below path whether AL_CHPAC xml is created or not c:\Program Files (x86)\Siemens\STEP7\S7DATA\driver\action\09000000 Hope it helps you! |
11/19/2021 5:48 AM | |
Joined: 1/11/2019 Last visit: 4/23/2024 Posts: 684 Rating: (139) |
Yes! It should created automatically |
Follow us on