11/12/2019 9:19 AM | |
Joined: 2/20/2014 Last visit: 9/17/2024 Posts: 396 Rating: (38) |
Hi, If you have are having Version 8.0 installed (full version not demo version then it should not be a problem for you to update the Version 8.0 to 8.2.1 (latest), you can just download the update from this link: https://support.industry.siemens.com/cs/ww/en/view/109767413 . |
Last edited by: RKBIS at: 11/12/2019 09:19:49Last edited by: Jen_Moderator at: 11/12/2019 12:19:32Optimized link. |
|
11/12/2019 9:21 AM | |
Joined: 12/18/2014 Last visit: 9/24/2024 Posts: 33829 Rating: (4204)
|
Only when the LOGO!s are not FS4-LOGO!. If the LOGO!s are FS4 types, then you Need LSC V8.1 or higher. But can make a upgrade for free from V8.0 to V8.2.1. You can download the upgrade from this website: LOGO! Soft Comfort V8.2 SP1 (download, notes, instructions) If you have download the complete upgrade (1,3 GB), start the setup file "install.htm" in the folder "LOGO V8_2 SP1 complete\LSC_V8_2_SP1 Upgrade\LSC_V8_2_SP1_Installers". |
Follow us on