9/27/2019 8:41 AM | |
Joined: 10/22/2011 Last visit: 8/26/2024 Posts: 299 Rating: (1) |
can I access PAC3200 on browser without powermanager software? |
9/27/2019 8:51 AM | |
Joined: 2/24/2015 Last visit: 1/25/2023 Posts: 306 Rating: (77) |
Display data from the PAC3200 in a browser without software - no. You need some kind of software that polls the PAC3200 and can display the data in the form of HTML pages. With PowerManager, you can collect data from the PAC3200. But as far as I remember, you can only display data on the local PC, there is no web server support there. If you need to display data via the web, see Energy Manager. |
9/27/2019 9:26 AM | |
Joined: 2/24/2015 Last visit: 1/25/2023 Posts: 306 Rating: (77) |
Yes. Trial licenses are available for these software. You can install and decide what is best suited to you. |
Follow us on