10/20/2017 11:51 AM | |
Posts: 531 Rating: (34) |
On linux samba is used to connect to a windows share. Is samba available on the iot device? |
10/24/2017 11:09 AM | |
Joined: 4/28/2015 Last visit: 4/30/2024 Posts: 3345 Rating: (377)
|
Hi, for accessing a Windows Shared Folder with Linux there is the package "cifs-utils". I've found a tutorial here: https://www.howtogeek.com/176471/how-to-share-files-between-windows-and-linux/ It is possible to integrate this package to the IOT2000 image. I did not found a specific node for this topic. But it is possible to call cifs-utils via exec node. I have to try this. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
10/27/2017 9:28 AM | |
Joined: 4/28/2015 Last visit: 4/30/2024 Posts: 3345 Rating: (377)
|
Hi all, if you do not have the possibility to build your own image you can build this package from its sources directly on the IOT2000. Download the latetst release of "cfis-utils" on https://github.com/Distrotech/cifs-utils/releases as tar.gz and copy this file to your IOT2000 (e.g using WinSCP). Then extract it with the command
and navigate to the extracted folder and execute the following commands:
Then you can use this functionality without building your own image Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
10/27/2017 4:18 PM | |
Joined: 3/17/2014 Last visit: 1/15/2024 Posts: 53 Rating: (12) |
Hi, attached you will find a step-by-step PDF guide with the same instruction of the bergmanu post. Hope that would be useful to everybody. Best Regards AttachmentHow to share files between Windows OS and IOT2040.pdf (1091 Downloads) |
This contribution was helpful to3 thankful Users |
Follow us on