9/16/2010 9:13 PM | |
Posts: 29 Rating: (0) |
Dear Experts, i have a S5 135U/155U cpu 928b If I power up the system the Run led is off .QVZ & BASP led is on. Digital Input led is ON but All digital output led is off i connect step5 with cpu. upload my backup program (s5d). no problem to upload,but still same error. Here is the photo-- CPU (see CPU.jpg in attachment) Digital input and output card.JPG (seeDigital input and output card.JPGin attachment) Error (see Error1.jpg in attachment) Error (seeError2.jpgin attachment) My Zennon SCADA is working fine. Now, Please, tell me, is it a hardware fault?? and how could i find out the faulty card? Thanks in Advance ISteak Attachmentpictures.zip (684 Downloads) |
Last edited by: O_Moderator at: 9/19/2010 9:54 AM |
|
9/16/2010 10:11 PM | |
Joined: 7/28/2010 Last visit: 3/18/2024 Posts: 184 Rating: (11) |
Isteak, Have you tried to do a cold restart? Please take a look at the attached file. Regards, Behnam www.sigmaprocess.ca/blog AttachmentCPU928-Cold Restart.pdf (1078 Downloads) |
9/16/2010 10:17 PM | |
Posts: 29 Rating: (0) |
yes i already try cold restart |
9/16/2010 10:29 PM | |
Joined: 7/28/2010 Last visit: 3/18/2024 Posts: 184 Rating: (11) |
Isteak, Check the ISTACK and see what the error is. Regards, Behnam www.sigmaprocess.ca/blog |
9/16/2010 10:49 PM | |
Posts: 29 Rating: (0) |
i am new on it a already upload the link of istack image PLS explain more details |
9/16/2010 11:51 PM | |
Joined: 7/28/2010 Last visit: 3/18/2024 Posts: 184 Rating: (11) |
Isteak, Check out Chapter 17 form the attached manual for Step5 V7.2 Regards, Behnam www.sigmaprocess.ca/blog AttachmentS5 V7.2.pdf (867 Downloads) |
9/17/2010 9:34 PM | |
Posts: 29 Rating: (0) |
from my s5d program it has 316 blocks if i transfer all block to PLC Stop, BASP, QVZ Led is ON and all output led is off but input led is on if i deleteOB13 & OB20 blockfrom PLC then, Stop & QVZ led is off. Run & BASP LED is ON (see attached s5d on zip) i already try cold warm reset now can you tell me how can i solve my problem?? which card is faulty digital input card or digital output card or...........?? i checked 24v in output it is all right but why there is no led on in digital output? if 1 digital output card is faulty then every digital output card willstop working?? PLEASE TELL ME HOW CAN I SOLVE MY PROBLEM?? THANKS ISTEAK Attachment51170EST.zip (496 Downloads) |
Follow us on