5/12/2021 11:40 AM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi, You would need to insert a dummy step before the simultaneous steps. Then you would have to save the dummy step and in resume let it return to the dummy step. |
If I could help you, you can use the RATE button. Thank you. |
|
5/17/2021 8:17 PM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi, You can set a bit variable (bit memory) in the middle of the step and when you resume, you go to the dummy step and insert a few jumps. In one of the jumps , check the bit memory if it is set and jump to the step you want. You will have to make sure it can never fail otherwise the SFC would hang if you do something wrong when using simultaneous steps. But this is something you can try. Maybe another way is changing the function , removing the simultaneous steps and rethink the functionality? You could share the functionality, try to rethink this together? |
Last edited by: Oreca at: 05/17/2021 20:52:33If I could help you, you can use the RATE button. Thank you. |
|
Follow us on