11/9/2018 9:00 AM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (375)
|
Hi, the problem is that your eth0 and yout wlan0 are in the same network (192.168.1.3 and 192.168.1.4). The two interfaces have to be in different networks like 192.168.1.3 and 192.168.2.4 You can't connect the IOT with two interfaces to the same router. A more detailed descrition why this is not possible can be found here. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to1 thankful Users |
Follow us on